Other Parts Discussed in Thread: OMAP-L137
Where can I go to find out how the physical memory on the OMAP-L137 is divided between the ARM and DSP cores? I know that the boot argument "mem=32M" specifies that the ARM core can only use the lowest 32MB (0xC000 0000 to 0xC1FF FFFF). I have also found some indications that the DSP/Link memory is the highest ~2MB on the board (although I am not sure how to check this myself, I found a sample memory map someone else posted).
This would seem to suggest that the ~30MB from 0xC200 0000 to 0xC3E0 0000 is free to be used. Can I just write values and read values to these locations in the memory directly from the DSP core? Do I need to use CMEM to do this? Or is it possible for me to do so directly.
Thanks