Hi
I have a problem when Iam setting brightness in android system. I am using DMTIMER10_PWM of omap4460
to generate 15 KHz for lcd-backlight. Everything is fine when I setting brightness 0~254 except that the brightness 255.
Sometimes omap4460 can generate PWM signal, but sometimes it can not generate PWM signal. By the way, I set
the PWM signal of voltage is always high when I set brightness 255. Is there any protection when the omap4460 generate
signal when voltage is always high??
Thank you
Jaden