Other Parts Discussed in Thread: SYSCONFIG
Hi all ,
I am working on porting MIPI DSI LCD panel on a custom board with OMAP4460. I am facing problems in clock settings. The pixel clock according to data sheet is 154MHz. Panel resolution is 1920x1280. SYS_CLOCK is 38.4MHz. Data rate is given 925MHz. RGB888(24 bits per pixel) and i am using 4 data lanes of DSI1 in command mode. From OMAP4460 Programming manual version F, Figure 10-152 we are following the algorithm. PLL_CLK should be less than 186MHz. How to get the values for pclk_div, lclk_div, regn, regm, regm_dispc, regm_dsi and lp_clk_div. I have tried with a set of values bu it is failing.
.clocks = {
.dispc = {
.channel = {
.lck_div = 1,
.pck_div = 2,
.lcd_clk_src = OMAP_DSS_CLK_SRC_DSI_PLL_HSDIV_DISPC,
},
.dispc_fclk_src = OMAP_DSS_CLK_SRC_FCK,
},
.dsi = {
.regn = 20,
.regm = 240,
.regm_dispc = 3,
.regm_dsi = 3,
.lp_clk_div = 10, /* LP Clock = 8.64 MHz */
.dsi_fclk_src = OMAP_DSS_CLK_SRC_DSI_PLL_HSDIV_DSI,
},
},
.channel = OMAP_DSS_CHANNEL_LCD,
.skip_init = false,
};
Can you please suggest on this.
Thanks
Abhijit