Hi All,
I am confused with cycles consumed [concept]
1. According to the document [Table 25][c66x Throughput performance guide],DirectIO: - 4096 bytes of packet, Total time taken [No time units mentioned in the .pdf] is around 40067.
whereas in tput_benchmarking example project [MCSDK .21]: - directioIO Nwrite [4096 bytes], average cycles is just 3455 cycles.
2. According to the document [c66x Throughput performance guide], Type 11 : - 4096 bytes of packet, average cycles consumed [88997],
whereas in tput_benchmarking example project [MCSDK .21]: - Type11 [4096 bytes], average cycles is around 4587 Average cycles.
can some Ti member please help me in understanding these two figures [one in .pdf throughput user guide and other one obtained through tput_benchmarking example project].
tput_benchmarking are for loopback versus c66x throughput performance benchmarking[this i assume is measured from board to board].please clarify
i am running this test [loopback] on c6670 board with mcsdk .21 and ccsv5.
Thanks
RC Reddy