This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Examples of EVM6678L board



Hi , 

I have purchased the above mentioned kit and with the provided CD I have installed CCS 5.0.1 but there are only examples related with MSP430 no example project

is present related to EVM6678L board. From where can I get the exmaples reagrding this multicore dev kit.

with regards,

Muhammad Faisal 

  • Muhammad Faisal,

    First, you should update to the latest CCSv5. Go to the Wiki and search for CCSv5 and you will find a link from which you can download the latest release. There is no license fee for using CCSv5 with your EVM6678L through the on-board emulator or when using the simulator.

    Then, you should download the latest MCSDK 2.x, also from the Wiki. It contains numerous examples for the EVM6678L.

    Regards,
    RandyP