Other Parts Discussed in Thread: AM3874
Hi,
I have one question from our customer.
Accroding to the Table 7-9 in 7.3.18 Reset Electrical Data/Timing of datasheet(sprs695a), it is specified that " th(BOOT)" (= Hold time, BTMODE[15:0] pins valid after xPOR high or xRESET high) is 0 ns (min ). But maximum value is not written in Table 7-9.
I know the value of maximum for the hold time is not needed usually. But our customer will connect one ASIC device to GPMC port. So ASIC device must output hi-z level signal until BTMODE port output. How is maximum value for "th(BOOT)"?
Or, according to the table 7-10 in 7.3.18 section of datasheet, it is specified that "td(RSTH-IOFUNC)" (= Delay time, xRESET high or xPOR high to all I/Os exiting their reset state). this timing is only specified the maximum value. How is minimum value for "td(RSTH-IOFUNC)"? If this minimum value is specified, the collision of ARM output and ASIC output can be avoided.
Please let me know which one value "the(BOOT)" maximum or "td(RSTH-IOFUNC)" minimum.
Best regards,
Michi