This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMMC connect to the mmc0



Hi,

AM335x TRM shows

An MMC/SD card can be connected to the MMC0 interface typically through a card cage.
An eMMC/eSD/managed NAND memory device can be connected to MMC1 interface.
Note:
• The ROM Code does not handle the card detection feature on card cage.
• If MMC1 is used the GPMC interface is not usable, due to pin muxing options.
• MMC1 supports sector mode without querying the card.

I don’t quite understand about this.

Can I connect a emmc to the mmc0 for boot?