For the C6672 datasheet power sequencing on p115-116. I have some queries here.
1. Only 2 clk is shown on p115 (SYSCLK1 and DDRCLK), but p116 refers to the clock drivers should be enabled once CVDD is valid. The clock drivers refer to the 6 clk (CORECLK, PASSCLK, DDRCLK, MCMCLK, PCIECLK, SRIOSGMIICLK)?
2. What does core AVS mean?
3. CVDD=core AVS and CVDD1=core constant?
4. static state => one leg must be high, one leg must be low?
5. RESETSTATz is driven low once the DVDD18 supply is available from p116. But from p115, the RESETSTATz is always low? Is it a drawing typo?
6. What is the clear indication of power stabilization phase and device initialization phase? From p115, it seems to be 1 vertical line. From p116, the power stabilization seem to end when PORz goes high. device initialization starts when SYSCLK and DDRCLK goes toggling. Another interpretation I get from p116 is power stabilization ends when the SYSCLK and DDRCLK starts toggling and device initialization starts when PORz goes high. May I know which interpretation is correct?
7. Why is the maximum clock period 33.33nsec => frequency=30MHz?
8. What is the efuse farm scan?