This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 not booting up.

Other Parts Discussed in Thread: OMAP-L138, AM1808

I am using OMAP-L138 and writing images in nand using Lauterbach. But board is not booting up and giving me an error

Booting with TI UBL

Device OPP (300MHz, 1.2V)

 

U-Boot 2012.04.01-svn23 (Jun 19 2012 - 16:13:42)

 

I2C:   ready

DRAM:  128 MiB

WARNING: Caches not enabled

NAND:  512 MiB

Bad block table found at page 262080, version 0x01

Bad block table found at page 262016, version 0x01

*** Warning - bad CRC, using default environment

 

In:    serial

Out:   serial

Err:   serial

SF: Detected M25P64 with page size 64 KiB, total 8 MiB

Net:   DaVinci-EMAC

Hit any key to stop autoboot:  0

 

Loading from nand0, offset 0x100000

NAND read from offset 100000 failed -74

** Read error

Wrong Image Format for bootm command

ERROR: can't get kernel image!

U-Boot >

When i tried to load the same image using tftp the board is booting up.

 

Thanks in advance.