This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does 4AI.1.5 OMAP4 ICS release on Blaze comply CDD ?



Hi All,


Does new 4AI.1.5 OMAP4 ICS release (http://omappedia.org/wiki/4AI.1.5_OMAP4_Icecream_Sandwich_Release_Notes) 
comply with the Compatibility Definition Document (CDD) ?

Regards.
Krt

  • Hi Krt,

    As per the CTS results report for 4AI.1.5 OMAP4 ICS release, the pass rate is around 99.90% and hence complies with the CDD for majority of the test cases. These are the comments from our test team in regards to the CTS results.

    Please note that several tests were added in CTS 4.0.3 R3 in comparison to R2, keep it in mind while reviewing comparisons to previous release executed on R2.

    Thanks & Best Regards,

    Venkat