This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Incompatible use of package...

Other Parts Discussed in Thread: SYSBIOS, OMAP-L138

We have been building SYSBIOS apps for awhile now.  Today we get the following error:

Description Resource Path Location Type
incompatible use of package 'ti.platforms.expOMAPL138' [in C:/TI/xdctools_3_23_00_32/packages/ti/platforms/expOMAPL138/]: version of the loaded package 'ti.platforms.expOMAPL138' is [], while 'ti.sysbios' [in C:/TI/bios_6_33_01_25/packages/ti/sysbios/] was built with 'ti.platforms.expOMAPL138' [1, 0, 0, 1323401440189] .xdchelp /SYSBIOS_ARM_configuration 156 C/C++ Problem

We have not upgraded anything recently and we have built SYSBIOS as early as yesterday successfully...

Where do we start to look to find the issue?

We have SYSBIOS 6.33.0019, 6.33.0125, and 6.33.0439.  Same error for all 3.

XDCtools we are useing 3.23.0.32.  We tried to go to 3.23.3.53 but there seems to be libraries that are not built for the OMAP-L138.

Compiler is v4.9.5 (ARM).  We also have 4.9.4 and 4.9.1 and all give the same errors.

CCS is 5.2.0.00070

Thanks,