This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Exporting graphical display from one AM1808 to another?

Other Parts Discussed in Thread: AM1808

Hi,

I have an AM1808 connected to a graphical LCD running a Qt based application (as in the LogicPd AM1808 experimenters kit).  What I would like to do is to export the graphical display to a second AM1808 connected to an LCD via an ethernet connection between the two processors - in essence creating a remote display.  Is something like this possible / feasible using the AM1808, and if so what are my options?  In the end I want to replace the "source" AM1808 with a larger Sitara device without an LCD connected, but I want to keep the AM1808 based remote display. 

Thanks!

Niki