This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

h263 encoder setting

hi,I meet a problem.

have someone to help me?


I use DVRRDK version 02.00.00.23 to test codec.
because DVRRDK do not support mpeg4 encoding and h263 encoding,I add some code and integrate REL.500.V.MPEG4.E.SP.IVAHD.01.00.00.05 to enc link to let DVRRDK encoding mpeg4 and h.263.
the application can generate mpeg4 and h263 bitstream well,
but I can not distinguish the h263 encoder setting.

the REL.500.V.MPEG4.E.SP.IVAHD.01.00.00.05 define these parameters for h263 encoder.

  IMPEG4ENC_H263_LEVEL_10 = 10,     /**< H263 Baseline Profile Level 10 */
  IMPEG4ENC_H263_LEVEL_20 = 20,     /**< H263 Baseline Profile Level 20 */
  IMPEG4ENC_H263_LEVEL_30 = 30,     /**< H263 Baseline Profile Level 30 */
  IMPEG4ENC_H263_LEVEL_40 = 40,     /**< H263 Baseline Profile Level 40 */
  IMPEG4ENC_H263_LEVEL_45 = 45,     /**< H263 Baseline Profile Level 45 */
  IMPEG4ENC_H263_LEVEL_50 = 50,     /**< H263 Baseline Profile Level 50 */
  IMPEG4ENC_H263_LEVEL_60 = 60,     /**< H263 Baseline Profile Level 60 */
  IMPEG4ENC_H263_LEVEL_70 = 70      /**< H263 Baseline Profile Level 70 */

which is in range of h263?
which is in range of h263+?

I only know the define below.

The original H.263 specified the following annexes:
    Annex A – Inverse transform accuracy specification
    Annex B – Hypothetical Reference Decoder
    Annex C – Considerations for Multipoint
    Annex D – Unrestricted Motion Vector mode
    Annex E – Syntax-based Arithmetic Coding mode
    Annex F – Advanced Prediction mode
    Annex G – PB-frames mode
    Annex H – Forward Error Correction for coded video signal

H.263v2 (H.263+)
    Annex I – Advanced INTRA Coding mode
    Annex J – Deblocking Filter mode
    Annex K – Slice Structured mode
    Annex L – Supplemental Enhancement Information Specification
    Annex M – Improved PB-frames mode
    Annex N – Reference Picture Selection mode
    Annex O – Temporal, SNR, and Spatial Scalability mode
    Annex P – Reference picture resampling
    Annex Q – Reduced-Resolution Update mode (see implementors' guide correction as noted below)
    Annex R – Independent Segment Decoding mode
    Annex S – Alternative INTER VLC mode
    Annex T – Modified Quantization mode
    Annex X – Profiles and levels definition