I was able to boot android on Da Vinci 8148, everything is working except the audio , which seems to be very low , I have heard people saying that it can be rectified/./or configured using alsa mixer , but on android if i type alsamixer or amixer on android terminal it says command not found. the asound.conf is not present in the specified directory and vene if i put some asound.conf file it hangs the android bootup, wat should i do