Hi,
I wanted to use the SD feature on TMS320DM36x DVRRD Rev2.1B board.
The board has not the SD slot. I expanded the SD slot to SD0 interface. (The SD0/1 has not the detect pin.)
I used the DM368_DVRRDK_v2.1 package. The UBL and U-boot of SD boot card could run from the expanded SD slot.
But Linux kernel could not discover the SD card. I found the SD/MMC is not support from build log.
How to modify SW or HW for SD enable?