This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem using DM6437 EVM with CCS 3.3

Hi,

We are starting evaluation with the DM6437 EVM purchased recently.
there are problems with the bundled CCS 3.3 and the on-board emulator.
after loading the example projects from "dvsdk_1_11_00_00" (like audio_video_encdec),
when we press the Run button, the processors seems to be freezed and
the output video is also freezed.
The board comes to normal condition only after resetting the board through power cycle.
(even it is similar in case of XDS510 emulator)
There are cases when the example program runs successfuly but most of
the time it won't.

But, when we try the same example projects(.out files) with CCSv5
it works fine without a problem.

We wonder this could be a problem with the CCS 3.3.
We are using 3.3 only bcos the example codes are built on CCS 3.3.

has anybody experienced similar issue with the EVM?
and also please let me know if anybody has the example codes ported for CCSv5.

Regards.
paddu