This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 EDMA Interrupts in StarterWare 1.20.03.03

Hello,

In the C6748 Technical Reference Manual (http://www.ti.com/lit/ug/spruh79a/spruh79a.pdf) page 501 references interrupts 

EDMA3_0_CC0_INT0, EDMA3_0_CC0_INT1, EDMA3_0_CC0_INT2, EDMA3_0_CC0_INT3, EDMA3_0_CC0_ERRINT and

EDMA3_1_CC0_INT0, EDMA3_1_CC0_INT1, EDMA3_1_CC0_INT2, EDMA3_1_CC0_INT3, EDMA3_1_CC0_ERRINT while in interrupts.h the EDMA interrupts available are:

/* EDMA Interrupts */
#define SYS_INT_EDMA3_0_CC0_INT1       8
#define SYS_INT_EDMA3_0_CC0_ERRINT 56
#define SYS_INT_EDMA3_0_TC0_ERRINT 57
#define SYS_INT_EDMA3_0_TC1_ERRINT 58
#define SYS_INT_EDMA3_1_CC0_INT1       91
#define SYS_INT_EDMA3_1_CC0_ERRINT 92
#define SYS_INT_EDMA3_1_TC0_ERRINT 93

 Page 531 shows dashed lines instead of actual interrupt number.  Are those not existent in CPU?

If we enable for CC0 both TC0 and TC1 how can I distinguish which transfer controller generated the interrupt? Is it with EDMA3GetIntrStatus and EDMA3IntrStatusHighGet?

I noticed in interrupts.h file that interrupts number 76, 77, 98 - 112, 114, 115, 124-128 are not defined. What interrupt sources correspond to?

Thank you in advance,

David.