I have a trouble to use XDS100 v2 in Ubuntu. I don't know if you heard this same problem from others before?
CCS reports
======
IcePick_D_0: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.0.681.0) ======
And I can't find serial port report from below:
======
halw@JONES-ubuntu:/opt/ti/ccsv5/ccs_base/common/uscif$ ./xds100serial Scanning for XDS100 emulators...
VID/PID Type Serial # Description
0403/a6d0 XDS100v1/v2 ? BeagleBon
======
I did use root to install the driver, but still same problem.
BTW, XDS100 v2 works fine in Windows.