This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to make use of hard as an option for -mfloat-abi...



Hi,

    I'm using Code Sorcery tool chain to build my C project ONLY for ARM Cortex-A8 processor on C6A816x EVM.

While building my project using the CS tool chain, for GCC option -mfloat-abi, I currently use softfp, but the GCC compiler manual says this for softfp option:

"`softfp' allows the generation of code using hardware floating-point instructions, but still uses the soft-float calling conventions."

In contrast it says that I could use hard as an option, for which the manual says:

"`hard' allows generation of floating-point instructions and uses FPU-specific calling conventions."

Apparently I would like to use hard as the option to build my project because it would then 'completely' make use of the FPU and its calling conventions. However when I do that, the project building won't succeed; the compilation succeeds but the linking fails with the following message:

/home/ti/CodeSourcery/Sourcery_G++_Lite/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/../../../../arm-none-linux-gnueabi/bin/ld: error: DSP.o uses VFP register arguments, ExampleProject does not

Can somebody throw some light on how I may make use of hard as an option for -mfloat-abi? Is there any other third party tool chain which I may make use of for this purpose?

Thank you!

  • Since you are using the CodeSourcery GCC toolchain and not the TI toolchain this question would be more appropriate at the device forum where the folks are more familiar with the CodeSourcery tools. I will move it to the device forum.