This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPMAP-L138 not booting up using tftp

Other Parts Discussed in Thread: OMAP-L138

Hi I am using OMAP-L138 board got bootup using files uImage and arago-base-tisdk-image-da850-omapl138-evm.tar.gz using nfs.

I read on ti forum that tar file cannot be use for tftp and nand boot. That's why I downloaded arago-demo-image-da850-omapl138-evm.ext2.gz from link http://arago-project.org/files/releases/2009.11/images/da850-omapl138-evm/

Then I tried to use both the files for tftpboot. But didn't got bootup.

bootcmd=nand read 0xc2600000 0xA00000 0x1300000; nboot 0xc0700000 0 0x100000; bootm

bootargs=mem=32M@0xc0000000 mem=64M@0xc4000000 console=ttyS2,115200n8 root=/dev/ram0 rw initrd=0xc2600000,13M ip=dhcp

U-Boot > tftp 0xc0200000 uImage
U-Boot > nand erase 0x100000 0x400000
U-Boot > nand write 0xc0200000 0x100000 0x400000

U-Boot > tftp 0xc2600000 arago-demo-image-da850-omapl138-evm.ext2.gz

U-Boot > nand erase 0xa00000 0x1300000

U-Boot > nand write 0xc2600000 0xa00000 0x1300000

After reset:

Booting with TI UBL
Device OPP (300MHz, 1.2V)

U-Boot 2012.04.01-svn30 (Jun 21 2012 - 12:22:36)

I2C:   ready
DRAM:  128 MiB
WARNING: Caches not enabled
NAND:  512 MiB
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
In:    serial
Out:   serial
Err:   serial
SF: Detected M25P64 with page size 64 KiB, total 8 MiB
Default using MAC address from environment
Default using MAC address from environment
Net:   DaVinci-EMAC
Hit any key to stop autoboot:  0

NAND read: device 0 offset 0xa00000, size 0x1300000
 19922944 bytes read: OK

Loading from nand0, offset 0x100000
   Image Name:   Linux-2.6.37+
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2152128 Bytes = 2.1 MiB
   Load Address: c0008000
   Entry Point:  c0008000
## Booting kernel from Legacy Image at c0700000 ...
   Image Name:   Linux-2.6.37+
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2152128 Bytes = 2.1 MiB
   Load Address: c0008000
   Entry Point:  c0008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

I made the kernal configuration changes also : disable MMC/SD support and enable NAND support.

After this nothing happens... Plesae help...