Other Parts Discussed in Thread: DM3730, OMAP3530
Hi,
Regarding DSPLink with linux 3.1.10
While running the ti dsplink eamples ....first time after board boot and inserting the module ....on DM3730 based boards....i am getting following warning...........
second times..onwards...this warning is not coming...........
Please let me know the solution.....
dvsdk_dm3730-evm_04_03_00_06_setuplinux ...................all the packages are taken from this
1.dspbios_5_41_03_17
2.dsplink_1_65_01_05_eng
linux version 3.1.10 used for building dsplink & lpm & cmem
/opt/ti_dsplink_examples # ./loopgpp loop.out 1000 1000
=============== Sample Application : LOOP ==========
==== Executing sample for DSP processor Id 0 ====
Entered LOOP_Create ()
Leaving LOOP_Create ()
Entered LOOP_Execute ()
[ 62.549468]
[ 62.549468] =============================================
[ 62.556762] [ INFO: possible recursive locking detected ]
[ 62.562438] 3.1.10-svn70 #1
[ 62.565399] ---------------------------------------------
[ 62.571075] DSPLINK_DPC_2/550 is trying to acquire lock:
[ 62.576690] (&obj->lock){+.+...}, at: [<bf011fcc>] SYNC_SpinLockStartEx+0x14/0x20 [dsplinkk]
[ 62.585906]
[ 62.585906] but task is already holding lock:
[ 62.592041] (&obj->lock){+.+...}, at: [<bf011fcc>] SYNC_SpinLockStartEx+0x14/0x20 [dsplinkk]
[ 62.601196]
[ 62.601196] other info that might help us debug this:
[ 62.608093] Possible unsafe locking scenario:
[ 62.608093]
[ 62.614349] CPU0
[ 62.616912] ----
[ 62.619476] lock(&obj->lock);
[ 62.622802] lock(&obj->lock);
[ 62.626129]
[ 62.626129] *** DEADLOCK ***
[ 62.626129]
[ 62.632385] May be due to missing lock nesting notation
[ 62.632385]
[ 62.639556] 1 lock held by DSPLINK_DPC_2/550:
[ 62.644134] #0: (&obj->lock){+.+...}, at: [<bf011fcc>] SYNC_SpinLockStartEx+0x14/0x20 [dsplinkk]
[ 62.653717]
[ 62.653717] stack backtrace:
[ 62.658386] [<c001be9c>] (unwind_backtrace+0x0/0x130) from [<c0092e18>] (__lock_acquire+0x18f0/0x1a88)
[ 62.668212] [<c0092e18>] (__lock_acquire+0x18f0/0x1a88) from [<c0093590>] (lock_acquire+0x98/0x120)
[ 62.677764] [<c0093590>] (lock_acquire+0x98/0x120) from [<c046d2fc>] (mutex_lock_interruptible_nested+0x5c/0x38c)
[ 62.688720] [<c046d2fc>] (mutex_lock_interruptible_nested+0x5c/0x38c) from [<bf011fcc>] (SYNC_SpinLockStartEx+0x14/0x20 [dsplinkk])
[ 62.701385] [<bf011fcc>] (SYNC_SpinLockStartEx+0x14/0x20 [dsplinkk]) from [<bf004930>] (IPS_notify+0x88/0x1ac [dsplinkk])
[ 62.713104] [<bf004930>] (IPS_notify+0x88/0x1ac [dsplinkk]) from [<bf00b0a8>] (ZCPYDATA_send+0x100/0x18c [dsplinkk])
[ 62.724365] [<bf00b0a8>] (ZCPYDATA_send+0x100/0x18c [dsplinkk]) from [<bf00b474>] (ZCPYDATA_dpc+0x340/0x3a8 [dsplinkk])
[ 62.735931] [<bf00b474>] (ZCPYDATA_dpc+0x340/0x3a8 [dsplinkk]) from [<bf011268>] (DPC_Callback+0xa0/0xec [dsplinkk])
[ 62.747131] [<bf011268>] (DPC_Callback+0xa0/0xec [dsplinkk]) from [<c007b124>] (kthread+0x80/0x88)
[ 62.756622] [<c007b124>] (kthread+0x80/0x88) from [<c00159d8>] (kernel_thread_exit+0x0/0x8)
Transferred 1000 buffers
Leaving LOOP_Execute ()
Entered LOOP_Delete ()
Leaving LOOP_Delete ()
====================================================
Awaitng for the positive response
Regards
Alex