Hello everyone,
I have downloaded the pre-built EtherCAT demo application on the TI ICE board (SDK 1.00.00.03) . I'm using the open source IgH EtherCAT Master for Linux [1]. The master detects the slave and all its PDO entries. I'm also able to configure the PDO mapping (I think so because the library doesn't give me any error on that). However, the ICE board doesn't seems to read/write the process data (working counter is always 0).
I also briefly tried the Simple Open EtherCAT Master (SOEM [2]) using the bundled 'simple_test'. This test application should find and configure slaves (which seems to be successfuly completed) and print all process data. However, as with the IgH Master, the working counter is never updated.
Before doing any further investigation, does anyone has already tested the demo application with the IgH or SOEM Master stack?
It seems that I'm not the only person who had this problem (http://lists.etherlab.org/pipermail/etherlab-users/2012/001728.html) but so far we didn't find the problem.
Thank you,
Philippe Hamelin