This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what's the proper procedure to manually load firmware/kernel modules?



I am trying ubuntu12.04 armhf on DM8148EVM, so I have to manually load all the TI modules(EZSDK5.04)

This is what i did

insmod syslink.ko
sudo firmware_loader 1 /usr/share/ti/ti-media-controller-utils/dm814x_hdvicp.xem3 start
sudo firmware_loader 2 /usr/share/ti/ti-media-controller-utils/dm814x_hdvpss.xem3 start
sudo modprobe vpss sbufaddr=0xBFB00000 mode=hdmi:1080p-60 i2c_mode=1

this is where the error starts:
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver

Did i miss anything? the kernel command line i used:

--no-log rootflags=barrier=1 console=ttyO0,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.vram=0:16M,1:16M,2:6M ip=192.168.1.169:192.168.1.1:192.168.1.1:255.255.255.0::eth0:

Please help!