This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Performance issue while encoding g.711 on dm365

Hi,


I am using DVSDK 3.0 with dm365, and testing TI's encode application.

When I just run either video or audio then applications works perfectly.
While running just audio encoder, ARM takes approximately 90% CPU.
I understood from other forums, it might be problem with cache enable.

 --------- Log -----------
Encode demo started.
@0,296,552us: [+6 T:0x4001f970] CE - Engine_init> CE debugging on (CE_DEBUG=1; allowed CE_DEBUG levels: 1=min, 2=good, 3=max)
ARM Load: 96% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 118 kbps Time: 00:00:02 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 98% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:04 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:06 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:08 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:10 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:12 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:14 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:16 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

ARM Load: 95% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 64 kbps Time: 00:00:18 Demo: Encode Display: D1 NTSC Video Codec: N/A Resolution: N/A Sound Codec: G.711 Speech Sampling Freq: 8 KHz samp rate

Please let me know
1) steps to enable cache and how to verify
2) how to sync audio and video.

Regards,
DS