Hi,
The on-board HUA demo has passed on EVM6678LE. I am trying to load small compiling program now. The system is CCS 5.2, Windows 7. In the configuration file (EVM6678Config.ccxml), I set Connection to: Blackhawk XDS560v2-USB Mezzanine Emulator, Device to: TMS320C6678. After I load the program (*.out), connect, the disassembly is stay at instruction: IDLE. Then, I try loading the MCSDK2.0 example Hello. It has the same problem,i.e. stay at instruction: IDLE. I notice that there is the original file with Hello example: C6678.cmd in the project. I don't see any problem with .ccxml and .cmd. What else should I check?
Thanks.