Hi, All!
On my custom board I changed memory map for 512MB systems, as stated in: http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map
While loading firmware I see this messages:
Loading HDVICP2 Firmware :FIRMWARE: I2cInit will be done by M3
FIRMWARE: memory map bin file: /usr/share/ti/ti-media-controller-utils/mm_dm81xxbm_512M.bin
FIRMWARE: isI2cInitRequiredOnM3: 1
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
*** ElfLoader_load: Failed to write args! (ensure .args section is big enough)
Error [0x0] at Line no: 1938 in file /home/karak/ezsdk_5_04_00_11/component-sources/syslink_2_10_03_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/procMgr/cc
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS Firmware :FIRMWARE: I2cInit will be done by M3
FIRMWARE: memory map bin file: /usr/share/ti/ti-media-controller-utils/mm_dm81xxbm_512M.bin
FIRMWARE: isI2cInitRequiredOnM3: 1
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
*** ElfLoader_load: Failed to write args! (ensure .args section is big enough)
Error [0x0] at Line no: 1938 in file /home/karak/ezsdk_5_04_00_11/component-sources/syslink_2_10_03_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/procMgr/cc
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
What does it mean this messages (selected bold font)?
How I can correct my system to solve this problem?
Thank you.
P.S. Sorry for my English.