Other Parts Discussed in Thread: 4460, DM3730
Dear All
How to add splash screen on u-boot on the omap 4460(DPI and HDMI)?
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason,
Can you refer to the following post below to get some guidelines on adding splash screen on u-boot for OMAP4460 (DPI & HDMI)?
http://e2e.ti.com/support/omap/f/849/t/107466.aspx
Thanks & Best Regards,
Venkat
Hi Venkat
I followied you provide web link.This is omap3 platform.
Is there a similar omap4 example?Because the two platforms register different too big.
Jason
Here is an example for OMAP4 that I made for configuring blaze tablet display for u-boot splash screen:
http://review.omapzoom.org/#/c/23975/
For DPI, the DISPC controller should be quite similar to this example, you would probably only need to configure the DISPC pins (data 23:0, vsync, hsync, de) on control module to make sure that they can output pixel data. Of course, you wouldn't be needing any DSI configuration. Also, if you don't want to use a PLL, you can use alternatively select a different clock source (e.g. DSS_CLK). Check DSS_CTRL register for this.
For HDMI, even that there are already some efforts to make it work, we don't have yet a working patch for this - hopefully we will have one soon. Even there, the DISPC part would look very similar; however, of course the HDMI module would need specific configuration.