When REG_IBANK_POS=0 and REG_EBANK_POS=0,
- What is the maximum number of banks interleaved within a device (per chip select)?
Is it all the banks?
- Is the interleaving of banks between the two chip selects possible?
The current AM335x is only one chip select (DDR_CSn[0])!
For the current AM335x which setting in the Address Mapping is available?
AM335x ARM Cortex-A8 Microprocessors (MPUs) Technical Reference Manual (Rev. F)
http://www.ti.com/lit/ug/spruh73f/spruh73f.pdf
7.3.3.4 Address Mapping
7.3.3.4.1 Address Mapping when REG_IBANK_POS=0 and REG_EBANK_POS=0
Best regards,
Daisuke