This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Qt Problem



I'm working on OMAPL137.

I download the QTOPIA-CORE-OPENSOURCE-SRC-4.2.2 and put it in the ~/target/opt, but errors occur after configuration:

ROOT@192.168.1.100:/OPT# CD /OPT/QTOPIA-CORE-OPENSOURCE-SRC-4.2.2
ROOT@192.168.1.100:/OPT/QTOPIA-CORE-OPENSOURCE-SRC-4.2.2# ./CONFIGURE -EMBEDDED ARM -QVFB

THIS IS THE QTOPIA CORE OPEN SOURCE EDITION.

YOU ARE LICENSED TO USE THIS SOFTWARE UNDER THE TERMS OF
THE GNU GENERAL PUBLIC LICENSE (GPL).

TYPE 'G' TO VIEW THE GNU GENERAL PUBLIC LICENSE.
TYPE 'YES' TO ACCEPT THIS LICENSE OFFER.
TYPE 'NO' TO DECLINE THIS LICENSE OFFER.

DO YOU ACCEPT THE TERMS OF THE LICENSE? YES

CREATING QMAKE. PLEASE WAIT...
G++ -C -O OPTION.O -PIPE -DQMAKE_OPENSOURCE_EDITION -I. -IGENERATORS -IGENERATORS/UNIX -IGENERATORS/WIN32 -IGENERATORS/MAC -I/OPT/QTOPIA-CORE-OPENSOURCE-P
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = c0004000
[00000000] *pgd=00000000
Internal error: Oops: 817 [#1]
Modules linked in: ipv6
CPU: 0
PC is at kmem_cache_free+0x38/0x78
LR is at kfree_skbmem+0xb0/0xbc
pc : [<c0095600>] lr : [<c0272330>] Not tainted
sp : c0351c60 ip : c0351c80 fp : c0351c7c
r10: 6301a8c0 r9 : 6401a8c0 r8 : c0682220
r7 : 0000001c r6 : c07c8c80 r5 : c07c8c80 r4 : c07c8c80
r3 : 00000000 r2 : c0401900 r1 : c07c8c80 r0 : c04d7b00
Flags: nZcv IRQs on FIQs on Mode SVC_32 Segment kernel
Control: 5317F
Table: C5008000 DAC: 00000017
Process swapper (pid: 0, stack limit = 0xc0350258)
Stack: (0xc0351c60 to 0xc0352000)
1c60: c027258c c0095564 c07c8c80 c07c8c80 c0351c94 c0351c80 c0272330 c00955d8
1c80: 0000001c c0683c60 c0351cac c0351c98 c0272418 c0272290 0000001c c054c2c0
1ca0: c0351cbc c0351cb0 c027247c c027234c c0351ccc c0351cc0 c0274980 c0272440
1cc0: c0351cfc c0351cd0 c02e224c c027497c c0351d24 ffffffff c0351d2c 00000024

.........

How to solve it?