This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CameraLink and CaptureLink?



hello,

anyone can tell me the difference of CameraLink and CaptureLink, which given in the 8127 IPNC RDK.

Thanks

  • CaptureLink is Link which configures and controls the Sensor. and creates the FVID2 frames for the rest of the flow.

    Where as, CameraLink is the link which controls ISS and ISP for the various processing.

    Regards,

    Venu

  • Hi Cai Jin,

    Capture link is actually used when you want to capture from the HD-VPSS capture ports (VIN0, VIN1). Capture link will interface to the HDVPSS drivers and configure the hardware for the capture.

    However, 

    Camera link is used when you would like to do ISS video port capture. Camera link will configure the ISS drivers for sensor configuration, ISP configuration (bayer to YUV) and also the ISS resizers for generation of scaled / non-scaled streams.

    Hope I gave you a brief description.

    Regards

    Rajat Sagar