Other Parts Discussed in Thread: OMAPL138, OMAP-L138
The OMAP TRM (spruh77a) states that only SD physical layer 1.1 is supported in hardware (implying SDSC cards upto 2GB). However the PSP driver notes (PSP 03.20 http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.20.00.11_Device_Driver_Features_and_Performance_Guide#Driver_Features_7) states that SDHC cards (upto 32GB) are also supported.
Please can you clarify the support offered on an OMAPL-138 running Linux / PSP? (my working assumption is that SDHC cards up to 32GB can be used, but only at the SDSC 25Mhz access speed @ 3.3v).