Hello,
Could you explain why C6678 EVM has coupling capacitors in RX path?
PCIe spec requires these capacitors only in TX path.
I'm asking because custom C6672 EP boards don't link up with DM814x EVM .
This custom board is designed as same as C6678 EVM, but doesn't have capacitors in RX path.
These custom C6672 boards work fine with x86 PCs in RC mode.
the DM814x EVM to be used works fine with C6678 EVM also.
Do you think the absence of capacitors is causing this issue?
Any other idea or better try adding capacitors?
Best regards,
N.Shinozaki