Other Parts Discussed in Thread: OMAPL138
Hi,
I have to slow down the SPI speed in OMAP L-137, where only PLL0 is present. Max. SPI1 CLK frequency 400kHz is required.
Is it really necessary to have fixed ratio SYSCLK2 = SYSCLK1 / 2?
What would happen if SYSCLK2 = SYSCLK1 / 3?
Is the only possibility to slow down the CPU operating frequency (i.e. maximum SYSCLK1 = 2 *256 * 400kHz = 204.8MHz )?
Thank you.
Radek