Hello evrybody,
I'm using a Ezdsp5515 kit and trying to make the MSC module work using the examples USB_MSC of CSL 2.50. the fact is that the POLL and FULLSPEED examples cannot find the SD card and the third one says the module is not initialez correctly. What can I do to make these example to work ? And what Part of the example do i need to add really in a full DSP/BIOS Project ?
Cheers
David