Hi,
I am Ana and i study engineering at Electronics and Telecommunication in Romania. I wanted to inform you that for my diploma thesis i made an application for Beagle Bone using the specifications from the standard IEEE 1588 version 2 Annexa F. I am really content with the results as i managed to synchronize two Beagle Bone devices by generating on each of them one signal with the frequency 1Hz. By doing so, the signal from the slave device is synchronized with the one from the master device.
I also wanted to thank you for the documentation available on the site.