hi,all
As the C6678 EVM's NAND Flash is slow. I want to change a NAND with the Micron's clearNAND.
But the SPRUGZ3a(C6678's EMIF User Guide) writes "The EMIF16 module does not support the following features:• NAND Flash that requires chip select to stay low during tR time for reads".
And the Micron's clearNAND"Enhanced ClearNAND Flash Memory MT29FEN32GDECAAXDQ, MT29FEN64GDKCAAXDQ" writes
"Asynchronous Data Input Data is written from DQ[7:0] to the data register of the selected volume on the rising edge of WE# when CE# is LOW, ALE is LOW, CLE is LOW, and RE# is HIGH."
Does that means the C6678 can't support the clearNAND?
And I want to know what's the use of the C6678's CE#.
thanks.