When I was using 6747 SPI1 as master in 4-pin mode with SCS[0] pin, I found this pin doesn't work. It held high all the time.
Then I try to test this pin, using it as an GPIO output, still it can't output low level. However, it worked well as a GPIO input.
I also tested SPI0, it's pins worked well.
I carefully checked the circuit and found no connecting error. I had 3 circuits of 2 different layout versions, they all exhibit such problem.
Could anyone help on this? Is it possible to be an bug of the chip?