This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the mean of XROT in XFMT register in McASP on DM646x



When I am reading the DM646x McASP datasheet, I get some confusion that the usage of XROT bits in XFMT register.

1.What's the different between Q31 fraction and Integer. Different internal numeric may affect the XROT mainly. How can I make sure the correct internal numeric on DM6467?

2.If I only set the XMASK register(not set XROT) like bolow.(slot = 16bits, I2S format)

mcasp_set_reg(dev->base + DAVINCI_MCASP_TXMASK_REG, 0x0000FFFF);

mcasp_set_reg(dev->base + DAVINCI_MCASP_RXMASK_REG, 0x0000FFFF);

then I use the aplay to test the driver, I coundn't heard any voice from the sound card.

but when I set the XROT bits like below:

mcasp_mod_bits(dev->base + DAVINCI_MCASP_TXFMT_REG, TXROT(rotate), TXROT(7));

mcasp_mod_bits(dev->base + DAVINCI_MCASP_RXFMT_REG, RXROT(rotate), RXROT(7));

mcasp_set_reg(dev->base + DAVINCI_MCASP_TXMASK_REG, 0x0000FFFF);

mcasp_set_reg(dev->base + DAVINCI_MCASP_RXMASK_REG, 0x0000FFFF);

everything is ok!

So, What exactly does XROT doing in my scenario?

thanks!