Other Parts Discussed in Thread: OMAPL138, OMAP-L137, TMS320C6747
Hello!
I am new in Softwaredevelopment for the OMAP Processor. I am currently working on a communication between the ARM and DSP Processors including loading and starting the DSP application from ARM side. I had working that easily using DSPLINK with DSP/BIOS 5.0. Now i have switched to SYS/BIOS 6 and the corresponding SYSLINK. Now i am searching for a SIMPLE example to get the same thing working with the updated environment. The suppied samples in the SYSLINK installation are compiling and working here fine. But how do i strip that down to a simple appliaction with one source file, one makefile and maybe one configuration file? The sample applications are a little bit complicated and scattered in my opinion.
So i am searching for a simple SYSLINK based example to load and start the DSP from the ARM side to get started with that topic. May be a CCS Project but may also be a standalone project.
Can anybody help me?
Best regards!