Hello!
I'm working with a custom design based on Craneboard schematic. Everything works fine but I have not a clue how to enable DVI output. I tried both AM3517EVM and Crane software but none of them provide DVI output out of the box. I suppose the problem is that no additional bootargs arguments are present in the u-boot environment. Can anybody list necessary arguments and their values so as I could boot the board and see a DVI display working immediately? For a example I used to work with the Beagleboard and it works just fine with both DVI and OEM LCD displays. I'm pretty sure that the success is behind the bootargs values. If I'm on the wrong way please fix me.
Max