This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 System trace with spectrum digital XDS560v2STM

Hi,

I Have a C6678 evaluation board and am attempting to debug some code with the system trace.

I cannot seem to figure out how to trace our code using the XDS560v2STM. The steps I have taken so far are:

- Load CCS5.1

- Start a debug session with the XDS560v2STM

- Connect to the non debuggable device CSSTM_0 (while leaving the C66xx_0 device with a receiver of 'None')

- In Tools -> Trace Control set up the XDS560v2STM on CSSTM_0

- use Tools -> Trace Analyser -> open trace conection in new view . To connect to the CSSTM_0 trace connection

- Run My code

At this point the code executes to completion, the Trace display shows three lines at time 0 and nothing else.

Am i doing something wrong? I have searched around but cannot find out what to do.

Regards,

Phil Dawson