This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6446 810 MHz Migration Issue

I am trying to migrate a 6446 to PLL1 of 810 Mhz from 513 MHz (it was at this speed due to legacy code).  It is mostly reliable, but I have an eventual lock-up when a lot of ethernet traffic is originating from the device.  I have found two clock dividers in the general network area and have scaled them accordingly.  These are:

EWINTTCNT - 0x3000 -> 0x4c00

CLKDIV in MDIO CONTROL - 0x4d -> 0x7a.

Beyond this, I've not touched PLL2 (DDR2 @ 135 MHz) and I've made some mods to the NOR-Flash EMIF chip select.  That's about it.  I'd appreciate it if anybody had any pointers.

Thanks.