Hi,
I am using IPNC_DM355 i can able to take the raw image how can i see the raw image.I cant able to open the picture as like as jpeg.I tried to open the raw image in the raw image viewer it is full of blue colour i cant able to see the image.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using IPNC_DM355 i can able to take the raw image how can i see the raw image.I cant able to open the picture as like as jpeg.I tried to open the raw image in the raw image viewer it is full of blue colour i cant able to see the image.
Hi,
You can use freely availble Image viewer like IrfanView which supports viewing the different RAW formats.
Regards,
Venu
Hi sir,
Thank you very much for your support it works i can able to see the raw image in the irfanview.
Hi sir,
I can able to see the raw image and i can view in the irfan view but it is in black and white not in color.
Hi Venkat,
The RAW image has got many formats, like what is the layout Gr R B Gb etc and also what is the bitdepth of each component whether 12-bit etc.
Irfan view provides option for the user to choose how the RAW file is. If you know the RAW format you can specify the exact option in Irfan View or else you might need to do some trial and error of selection the combinations of options.
Regards,
Venu
Dear sir,
Thank you very much for the relay.I attached the raw image and the capture application with this post.
/**+--------------------------------------------------------------------------+**
**| **** |**
**| **** |**
**| ******o*** |**
**| ********_///_**** |**
**| ***** /_//_/ **** |**
**| ** ** (__/ **** |**
**| ********* |**
**| **** |**
**| *** |**
**| |**
**| Copyright (c) 1998-2008 Texas Instruments Incorporated |**
**| ALL RIGHTS RESERVED |**
**| |**
**| Permission is hereby granted to licensees of Texas Instruments |**
**| Incorporated (TI) products to use this computer program for the sole |**
**| purpose of implementing a licensee product based on TI products. |**
**| No other rights to reproduce, use, or disseminate this computer |**
**| program, whether in part or in whole, are granted. |**
**| |**
**| TI makes no representation or warranties with respect to the |**
**| performance of this computer program, and specifically disclaims |**
**| any responsibility for any damages, special or consequential, |**
**| connected with the use of this program. |**
**| |**
**+--------------------------------------------------------------------------+**
*******************************************************************************/
/*******************************************************************************
* HEADER FILES
*/
#include <stdio.h>
#include <fcntl.h>
#include <string.h>
#include <getopt.h>
#include <stdlib.h>
#include <unistd.h>
#include <errno.h>
#include <sys/types.h>
#include <sys/time.h>
#include <sys/mman.h>
#include <sys/ioctl.h>
#include <fcntl.h>
#include <linux/fb.h>
#include <asm/types.h>
#include <time.h>
/* Kernel header file, prefix path comes from makefile */
#include <linux/videodev2.h>
//#include <media/tvp514x.h>
//#include <media/davinci/davinci_vpfe.h>
#include <video/davincifb.h>
//#include "osd16.h"
//#include "test_8.h"
/*******************************************************************************
* LOCAL DEFINES
*/
#define CAPTURE_DEVICE "/dev/video0"
#define WIDTH_PAL 720
#define HEIGHT_PAL 576
#define WIDTH_NTSC 720
#define HEIGHT_NTSC 480
//#define WIDTH_VGA 640 //works
//#define HEIGHT_VGA 480 // works
#define WIDTH_VGA 1280
#define HEIGHT_VGA 720
#define MIN_BUFFERS 2
#define UYVY_BLACK 0x10801080
/* Device parameters */
#define OSD0_DEVICE "/dev/fb/0"
#define OSD1_DEVICE "/dev/fb/2"
#define FBVID0_DEVICE "/dev/fb/1"
#define FBVID1_DEVICE "/dev/fb/3"
/* Function error codes */
#define SUCCESS 0
#define FAILURE -1
/* Bits per pixel for video window */
#define YUV_422_BPP 16
#define BITMAP_BPP_8 8
#define DISPLAY_INTERFACE "COMPOSITE"
#define DISPLAY_MODE_NTSC "NTSC"
#define DISPLAY_MODE_PAL "PAL"
#define round_32(width) ((((width) + 31) / 32) * 32 )
/* D1 screen dimensions */
#define VID0_WIDTH 720
#define VID0_HEIGHT 480
#define VID0_BPP 16
#define VID0_FRAME_SIZE (VID0_WIDTH*VID0_HEIGHT)
#define VID0_VMODE FB_VMODE_INTERLACED
#define VID1_WIDTH 720
#define VID1_HEIGHT 480
#define VID1_BPP 16
#define VID1_FRAME_SIZE (VID1_WIDTH*VID1_HEIGHT)
#define VID1_VMODE FB_VMODE_INTERLACED
#define OSD0_BPP 4
#define OSD0_WIDTH (round_32(240*OSD0_BPP/8) * 8/OSD0_BPP)
#define OSD0_HEIGHT 120
#define OSD0_FRAME_SIZE (OSD0_WIDTH*OSD0_HEIGHT)
#define OSD0_VMODE FB_VMODE_INTERLACED
#define OSD1_BPP 8
#define OSD1_WIDTH (round_32(240*OSD1_BPP/8) * 8/OSD1_BPP)
#define OSD1_HEIGHT 120
#define OSD1_FRAME_SIZE (OSD1_WIDTH*OSD1_HEIGHT)
#define OSD1_VMODE FB_VMODE_INTERLACED
/* position */
#define OSD0_XPOS 0
#define OSD0_YPOS 0
#define OSD1_XPOS 300
#define OSD1_YPOS 250
#define VID0_XPOS 0
#define VID0_YPOS 0
#define VID1_XPOS 0
#define VID1_YPOS 0
/* Zoom Params */
#define OSD0_HZOOM 0
#define OSD0_VZOOM 0
#define OSD1_HZOOM 0
#define OSD1_VZOOM 0
#define VID0_HZOOM 0
#define VID0_VZOOM 0
#define VID1_HZOOM 0
#define VID1_VZOOM 0
/* OSD window blend factor */
#define OSD1_WINDOW_BF 0
#define OSD1_WINDOW_CK 0
#define OSD1_CK 0
#define OSD0_WINDOW_BF 3
#define OSD0_WINDOW_CK 0
#define OSD0_CK 0
#define VIDEO_NUM_BUFS 3
#define OSD_NUM_BUFS 2
#define RED_COLOR 249
#define BLUE_COLOR 140 //blue color
#define RAM_CLUT_IDX 0xFF
#define BITMAP_COLOR 0x11
#define CURSOR_XPOS 100
#define CURSOR_YPOS 100
#define CURSOR_XRES 50
#define CURSOR_YRES 50
#define CURSOR_THICKNESS 1
#define CURSOR_COLOR 0xF9
#define ATTR_BLINK_INTERVAL 1
#define ATTR_BLEND_VAL 0xaa
#define ATTRIB_MODE "mode"
#define ATTRIB_OUTPUT "output"
#define LOOP_COUNT 50000
#define DEBUG
#ifdef DEBUG
#define DBGENTER printf("%s : Enter\n", __FUNCTION__);
#define DBGEXIT printf("%s : Leave\n", __FUNCTION__);
#define PREV_DEBUG(x) printf("DEBUG:%s:%s:%s\n",__FUNCTION__,__LINE__,x);
#else
#define DBGENTER
#define DBGEXIT
#define PREV_DEBUG(x)
#endif
#define CLEAR(x) memset (&(x), 0, sizeof (x))
//leon test
char rgb16[100];
char test_8[100];
/*******************************************************************************
* STRUCTURE DEFINITIONS
*/
struct buffer {
void *start;
size_t length;
};
struct vpbe_test_info {
int vid0_width;
int vid0_height;
int vid0_bpp;
int vid0_frame_size;
int vid0_vmode;
int vid1_width;
int vid1_height;
int vid1_bpp;
int vid1_frame_size;
int vid1_vmode;
int osd0_bpp;
int osd0_width;
int osd0_height;
int osd0_frame_size;
int osd0_vmode;
int osd1_bpp;
int osd1_width;
int osd1_height;
int osd1_frame_size;
int osd1_vmode;
int osd0_xpos;
int osd0_ypos;
int osd1_xpos;
int osd1_ypos;
int vid0_xpos;
int vid0_ypos;
int vid1_xpos;
int vid1_ypos;
int osd0_hzoom;
int osd0_vzoom;
int osd1_hzoom;
int osd1_vzoom;
int vid0_hzoom;
int vid0_vzoom;
int vid1_hzoom;
int vid1_vzoom;
int osd1_window_bf;
int osd1_window_ck;
int osd1_ck;
int osd0_window_bf;
int osd0_window_ck;
int osd0_ck;
int osd0_coloridx;
int osd1_coloridx;
int ram_clut_idx;
int bitmap_color;
int cursor_xpos;
int cursor_ypos;
int cursor_xres;
int cursor_yres;
int cursor_thickness;
int cursor_color;
int attr_blink_interval;
int attr_blend_val;
};
/*******************************************************************************
* FILE GLOBALS
*/
static struct vpbe_test_info test_data = {
VID0_WIDTH,
VID0_HEIGHT,
VID0_BPP,
VID0_FRAME_SIZE,
VID0_VMODE,
VID1_WIDTH,
VID1_HEIGHT,
VID1_BPP,
VID1_FRAME_SIZE,
VID1_VMODE,
OSD0_BPP,
OSD0_WIDTH,
OSD0_HEIGHT,
OSD0_FRAME_SIZE,
OSD0_VMODE,
OSD1_BPP,
OSD1_WIDTH,
OSD1_HEIGHT,
OSD1_FRAME_SIZE,
OSD1_VMODE,
OSD0_XPOS,
OSD0_YPOS,
OSD1_XPOS,
OSD1_YPOS,
VID0_XPOS,
VID0_YPOS,
VID1_XPOS,
VID1_YPOS,
OSD0_HZOOM,
OSD0_VZOOM,
OSD1_HZOOM,
OSD1_VZOOM,
VID0_HZOOM,
VID0_VZOOM,
VID1_HZOOM,
VID1_VZOOM,
OSD1_WINDOW_BF,
OSD1_WINDOW_CK,
OSD1_CK,
OSD0_WINDOW_BF,
OSD0_WINDOW_CK,
OSD0_CK,
BLUE_COLOR,
RED_COLOR,
RAM_CLUT_IDX,
BITMAP_COLOR,
CURSOR_XPOS,
CURSOR_YPOS,
CURSOR_XRES,
CURSOR_YRES,
CURSOR_THICKNESS,
CURSOR_COLOR,
ATTR_BLINK_INTERVAL,
ATTR_BLEND_VAL,
};
static int fdCapture = -1;
static struct buffer *buffers = NULL;
static int nBuffers;
static int nWidthFinal;
static int nHeightFinal;
static int quit;
static char *vid0_display[VIDEO_NUM_BUFS];
static char *vid1_display[VIDEO_NUM_BUFS];
static char *osd0_display[OSD_NUM_BUFS];
static char *osd1_display[OSD_NUM_BUFS];
static int fd_vid0, fd_vid1, fd_osd0, fd_osd1;
static struct fb_var_screeninfo vid1_varInfo, osd0_varInfo, osd1_varInfo,
prev_vid1_var, prev_osd0_var;
static struct fb_fix_screeninfo vid0_fixInfo, vid1_fixInfo, osd0_fixInfo,
osd1_fixInfo;
static int vid0_size, vid1_size, osd0_size, osd1_size;
static int stress_test = 1;
static int start_loopCnt = LOOP_COUNT;
static int rgb565_enable;
static int rgb565_enable_osd1;
static int display_out = 0;//leon 1;
static int save_frame = 1;
FILE *file_fp;
static int print_fn;// = 1;
#define CAPTURE_FILE "/mnt/mmc/capt_frame.raw"
/*******************************************************************************
* EXTERN VARIABLES
*/
extern int errno;
/*******************************************************************************
* LOCAL FUNCTION PROTOTYPES
*/
static void restore_config(void);
static int initialize_capture(v4l2_std_id * cur_std);
static int start_loop(void);
static int init_capture_device(void);
static int set_data_format(v4l2_std_id * cur_std);
static int init_capture_buffers(void);
static int start_streaming(void);
static int display_frame(char, void *);
static int flip_bitmap_buffers(int, int);
static int flip_video_buffers(int, int);
static int mmap_vid1(void);
static int mmap_osd0(void);
static int display_bitmap_osd0(void);
static int display_bitmap_osd1(void);
static int unmap_and_disable(char);
static int init_osd0_device(int, struct fb_var_screeninfo *);
static int init_vid1_device(int, struct fb_var_screeninfo *);
static int vpbe_UE_1(void);
static void close_all_windows(void);
static int open_all_windows(void);
static int change_sysfs_attrib(char *, char *);
/*******************************************************************************
* FUNCTION DEFINITIONS
*/
static void restore_config(void)
{
struct fb_cursor cursor_info;
DBGENTER;
cursor_info.enable = 0;
cursor_info.image.dx = CURSOR_XPOS;
cursor_info.image.dy = CURSOR_YPOS;
cursor_info.image.width = CURSOR_XRES;
cursor_info.image.height = CURSOR_YRES;
cursor_info.image.depth = CURSOR_THICKNESS;
cursor_info.image.fg_color = CURSOR_COLOR;
#if 0
if (ioctl(fd_vid1, FBIO_SET_CURSOR, &cursor_info) < 0) {
perror("\nFailed FBIO_SET_CURSOR");
return;
}
#endif
if (ioctl(fd_osd1, FBIOGET_FSCREENINFO, &osd1_fixInfo) < 0) {
perror("\nFailed FBIOGET_FSCREENINFO osd1");
return;
}
/* Get Existing var_screeninfo for vid0 window */
if (ioctl(fd_osd0, FBIOGET_VSCREENINFO, &osd0_varInfo) < 0) {
printf("\nFailed FBIOGET_VSCREENINFO");
return;
}
/* Modify the resolution and bpp as required */
osd0_varInfo.bits_per_pixel = 16;
/* Set vid0 window format */
if (ioctl(fd_osd0, FBIOPUT_VSCREENINFO, &osd0_varInfo) < 0) {
printf("\nFailed FBIOPUT_VSCREENINFO");
return;
}
osd0_display[0] =
(char *)mmap(NULL,
osd0_fixInfo.line_length * osd0_varInfo.yres_virtual,
PROT_READ | PROT_WRITE, MAP_SHARED, fd_osd0, 0);
osd1_display[0] =
(char *)mmap(NULL,
osd1_fixInfo.line_length * osd1_varInfo.yres_virtual,
PROT_READ | PROT_WRITE, MAP_SHARED, fd_osd1, 0);
vid1_display[0] =
(char *)mmap(NULL,
vid1_fixInfo.line_length * vid1_varInfo.yres_virtual,
PROT_READ | PROT_WRITE, MAP_SHARED, fd_vid1, 0);
memset(osd0_display[0], 0x00,
osd0_fixInfo.line_length * osd0_varInfo.yres_virtual);
memset(osd1_display[0], 0x11,
osd1_fixInfo.line_length * osd1_varInfo.yres_virtual);
memset(vid1_display[0], 0x80,
vid1_fixInfo.line_length * vid1_varInfo.yres_virtual);
munmap(osd0_display[0],
osd0_fixInfo.line_length * osd0_varInfo.yres_virtual);
munmap(osd1_display[0],
osd1_fixInfo.line_length * osd1_varInfo.yres_virtual);
munmap(vid1_display[0],
vid1_fixInfo.line_length * vid1_varInfo.yres_virtual);
system("cat /dev/zero > /dev/fb/2 2> /dev/null");
DBGEXIT;
}
/******************************************************************************/
static int initialize_capture(v4l2_std_id * cur_std)
{
int ret;
printf("initializing capture device\n");
init_capture_device();
#if 1
printf("setting data format\n");
ret = set_data_format(cur_std);
if (ret) {
printf("Error in setting capture format\n");
return ret;
}
#endif
printf("initializing capture buffers\n");
ret = init_capture_buffers();
if (ret) {
printf("Failed to initialize capture buffers\n");
return ret;
}
printf("initializing display device\n");
ret = start_streaming();
if (ret) {
printf("Failed to start capture streaming\n");
return ret;
}
return 0;
}
/******************************************************************************/
static int start_loop(void)
{
struct v4l2_buffer buf;
int FrmCntSave = 0;
static int captFrmCnt = 0;
char *ptrPlanar = NULL;
int dummy;
unsigned long StartTime, EndTime;
ptrPlanar = (char *)calloc(1, nWidthFinal * nHeightFinal * 2);
while (!quit) {
fd_set fds;
struct timeval tv;
int r;
if (stress_test) {
start_loopCnt--;
if (start_loopCnt == 0) {
start_loopCnt = 50;
break;
}
}
FD_ZERO(&fds);
FD_SET(fdCapture, &fds);
/* Timeout */
tv.tv_sec = 2;
tv.tv_usec = 0;
r = select(fdCapture + 1, &fds, NULL, NULL, &tv);
if (-1 == r) {
if (EINTR == errno)
continue;
printf("StartCameraCapture:select\n");
return -1;
}
if (0 == r)
continue;
if (display_out) {
/* Wait for vertical sync */
if (ioctl(fd_vid1, FBIO_WAITFORVSYNC, &dummy) < -1) {
printf("Failed FBIO_WAITFORVSYNC\n");
if (EAGAIN == errno) {
printf("disp_again\n");
continue;
}
return -1;
}
}
CLEAR(buf);
buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
buf.memory = V4L2_MEMORY_MMAP;
/* determine ready buffer */
if (-1 == ioctl(fdCapture, VIDIOC_DQBUF, &buf)) {
//leon if (EAGAIN == errno)
// printf("capt_again\n");
continue;
printf("StartCameraCaputre:ioctl:VIDIOC_DQBUF\n");
return -1;
}
#if 1
if (captFrmCnt >= 5) {
file_fp = fopen(CAPTURE_FILE, "wb");
if (file_fp == NULL) {
printf("Unable to open %s\n", CAPTURE_FILE);
}else if (save_frame) {
fwrite(buffers[buf.index].start,
1, (nWidthFinal * nHeightFinal * 2),
file_fp);
printf("Saved file %s\n", CAPTURE_FILE);
}
save_frame = 0;
fclose(file_fp);
quit = 1;
}
#endif
if (display_out) {
display_frame(VID1, buffers[buf.index].start);
display_bitmap_osd0();
}
captFrmCnt++;
if (captFrmCnt > FrmCntSave + 100 && captFrmCnt > 100){
EndTime = (unsigned long)time(NULL);
printf("frame rate = %3.2f\n", (float)(captFrmCnt -FrmCntSave) / ( EndTime - StartTime) );
StartTime = (unsigned long)time(NULL);
FrmCntSave = captFrmCnt;
}
if (print_fn)
printf("time:%lu frame:%u\n", (unsigned long)time(NULL), captFrmCnt);
/* requeue the buffer */
if (-1 == ioctl(fdCapture, VIDIOC_QBUF, &buf)) {
printf("StartCameraCaputre:ioctl:VIDIOC_QBUF\n");
return -1;
}
}
return SUCCESS;
}
/******************************************************************************/
static int init_capture_device(void)
{
struct v4l2_capability cap;
printf("entering init_capture_device\n");
#if 0
/* input-0 is selected by default, so no need to set it */
if ((fdCapture = open(CAPTURE_DEVICE, O_RDWR | O_NONBLOCK, 0)) <= -1) {
printf("InitDevice:open::\n");
return -1;
}
#endif
/* input-0 is selected by default, so no need to set it */
printf("fdCapture = open \n");
if ((fdCapture = open(CAPTURE_DEVICE, O_RDWR )) <= -1) {
printf("InitDevice:open:: fdCapture = %x\n",fdCapture);
return -1;
}
/* is capture supported? */
printf("fdCapture, VIDIOC_QUERYCAP \n");
if (-1 == ioctl(fdCapture, VIDIOC_QUERYCAP, &cap)) {
printf("InitDevice:ioctl:VIDIOC_QUERYCAP:\n");
return -1;
}
if (!(cap.capabilities & V4L2_CAP_VIDEO_CAPTURE)) {
printf("InitDevice:capture is not supported on:%s\n",
CAPTURE_DEVICE);
return -1;
}
/* is MMAP-IO supported? */
if (!(cap.capabilities & V4L2_CAP_STREAMING)) {
printf("InitDevice:IO method MMAP is not supported on:%s\n",
CAPTURE_DEVICE);
return -1;
}
return 0;
}
/******************************************************************************/
static int set_data_format(v4l2_std_id *cur_std)
{
// v4l2_std_id prev_std;
struct v4l2_format fmt;
unsigned int min;
struct v4l2_input input;
int temp_input;
// struct v4l2_cropcap cropcap;
// struct v4l2_fmtdesc fmt_desc;
#if 0
// first set the input
input.type = V4L2_INPUT_TYPE_CAMERA;
input.index = 0;
while (0 == ioctl(fdCapture,VIDIOC_ENUMINPUT, &input)) {
printf("input.name = %s\n", input.name);
//if (!strcmp(input.name, "COMPOSITE"))
// break;
input.index++;
}
if (-1 == ioctl (fdCapture, VIDIOC_S_INPUT, &input.index))
{
perror("Error:InitDevice:ioctl:VIDIOC_S_INPUT\n");
return -1;
}
printf ("InitDevice:ioctl:VIDIOC_S_INPUT, selected COMPOSITE INPUT input\n");
if (-1 == ioctl (fdCapture, VIDIOC_G_INPUT, &temp_input))
{
perror("Error:InitDevice:ioctl:VIDIOC_G_INPUT\n");
return -1;
}
if (temp_input == input.index)
printf ("InitDevice:ioctl:VIDIOC_G_INPUT, selected COMPOSITE INPUT input\n");
else {
printf ("Error: InitDevice:ioctl:VIDIOC_G_INPUT,");
printf("Couldn't select COMPOSITE INPUT input\n");
return -1;
}
#endif
#if 0
*cur_std = V4L2_STD_PAL;
if (-1 == ioctl(fdCapture, VIDIOC_S_STD, cur_std)) {
perror("set_data_format:ioctl:VIDIOC_S_STD\n");
return -1;
}
#endif
#if 0
if (-1 == ioctl(fdCapture, VIDIOC_QUERYSTD, cur_std)) {
perror("set_data_format:ioctl:VIDIOC_QUERYSTD:\n");
return -1;
}
if (*cur_std & V4L2_STD_NTSC)
printf("Input video standard is NTSC.\n");
else if (*cur_std & V4L2_STD_PAL)
printf("Input video standard is PAL.\n");
else if (*cur_std & V4L2_STD_PAL_M)
printf("Input video standard is PAL-M.\n");
else if (*cur_std & V4L2_STD_PAL_N)
printf("Input video standard is PAL-N.\n");
else if (*cur_std & V4L2_STD_SECAM)
printf("Input video standard is SECAM.\n");
else if (*cur_std & V4L2_STD_PAL_60)
printf("Input video standard to PAL60.\n");
else
return -1;
#endif
#if 0
/* select cropping as deault rectangle */
cropcap.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
if (-1 == ioctl(fdCapture, VIDIOC_CROPCAP, &cropcap)) {
printf("InitDevice:ioctl:VIDIOC_CROPCAP\n");
/* ignore error */
}
printf("Default crop capbility bounds - %d %d %d %d"
" ; default - %d %d %d %d \n",
cropcap.bounds.left, cropcap.bounds.top,
cropcap.bounds.width, cropcap.bounds.height,
cropcap.defrect.left, cropcap.defrect.top,
cropcap.defrect.width, cropcap.defrect.height);
printf("set_data_format:setting data format\n");
CLEAR(fmt_desc);
fmt_desc.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
printf("Available image formats at the capture driver :-\n");
while (0 == ioctl(fdCapture, VIDIOC_ENUM_FMT, &fmt_desc)) {
printf("fmt_desc.index = %d\n", fmt_desc.index);
printf("fmt_desc.type = %d\n", fmt_desc.type);
printf("fmt_desc.description = %s\n", fmt_desc.description);
printf("fmt_desc.pixelformat = %x\n", fmt_desc.pixelformat);
fmt_desc.index++;
}
/* Try format with minimum and maximum values */
CLEAR(fmt);
fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
fmt.fmt.pix.width = 1;
fmt.fmt.pix.height = 1;
fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_UYVY;
fmt.fmt.pix.field = V4L2_FIELD_ANY;
printf("*******TRY_FMT (Min resolution) values before calling ioctl*************\n");
printf("fmt.fmt.pix.width = %d\n", fmt.fmt.pix.width);
printf("fmt.fmt.pix.height = %d\n", fmt.fmt.pix.height);
printf("fmt.fmt.pix.field= %d\n", fmt.fmt.pix.field);
printf("fmt.fmt.pix.bytesperline = %d\n", fmt.fmt.pix.bytesperline);
printf("fmt.fmt.pix.sizeimage = %d\n", fmt.fmt.pix.sizeimage);
if (-1 == ioctl(fdCapture, VIDIOC_TRY_FMT, &fmt))
printf("Error:set_data_format:ioctl:VIDIOC_TRY_FMT\n");
printf("*******TRY_FMT values after calling ioctl*************\n");
printf("fmt.fmt.pix.width = %d\n", fmt.fmt.pix.width);
printf("fmt.fmt.pix.height = %d\n", fmt.fmt.pix.height);
printf("fmt.fmt.pix.field= %d\n", fmt.fmt.pix.field);
printf("fmt.fmt.pix.bytesperline = %d\n", fmt.fmt.pix.bytesperline);
printf("fmt.fmt.pix.sizeimage = %d\n", fmt.fmt.pix.sizeimage);
#endif
#if 0
CLEAR(fmt);
fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
fmt.fmt.pix.width = (1 << 15);
fmt.fmt.pix.height = (1 << 15);
fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_UYVY;
fmt.fmt.pix.field = V4L2_FIELD_ANY;
printf("*******TRY_FMT (Max resolution) values before calling ioctl*************\n");
printf("fmt.fmt.pix.width = %d\n", fmt.fmt.pix.width);
printf("fmt.fmt.pix.height = %d\n", fmt.fmt.pix.height);
printf("fmt.fmt.pix.field= %d\n", fmt.fmt.pix.field);
printf("fmt.fmt.pix.bytesperline = %d\n", fmt.fmt.pix.bytesperline);
printf("fmt.fmt.pix.sizeimage = %d\n", fmt.fmt.pix.sizeimage);
if (-1 == ioctl(fdCapture, VIDIOC_TRY_FMT, &fmt))
printf("Error:set_data_format:ioctl:VIDIOC_TRY_FMT\n");
printf("*******TRY_FMT values after calling ioctl*************\n");
printf("fmt.fmt.pix.width = %d\n", fmt.fmt.pix.width);
printf("fmt.fmt.pix.height = %d\n", fmt.fmt.pix.height);
printf("fmt.fmt.pix.field= %d\n", fmt.fmt.pix.field);
printf("fmt.fmt.pix.bytesperline = %d\n", fmt.fmt.pix.bytesperline);
printf("fmt.fmt.pix.sizeimage = %d\n", fmt.fmt.pix.sizeimage);
#endif
#if 0
if (*cur_std & V4L2_STD_NTSC) {
fmt.fmt.pix.width = WIDTH_NTSC;
fmt.fmt.pix.height = HEIGHT_NTSC;
} else {
fmt.fmt.pix.width = WIDTH_PAL;
fmt.fmt.pix.height = HEIGHT_PAL;
}
#endif
fmt.fmt.pix.width = WIDTH_VGA;
fmt.fmt.pix.height = HEIGHT_VGA;
fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_UYVY;
#if 1
fmt.fmt.pix.field = V4L2_FIELD_NONE;//leon V4L2_FIELD_INTERLACED;
if (-1 == ioctl(fdCapture, VIDIOC_S_FMT, &fmt))
printf("set_data_format:ioctl:VIDIOC_S_FMT\n");
#endif
#if 1
if (-1 == ioctl(fdCapture, VIDIOC_G_FMT, &fmt))
printf("set_data_format:ioctl:VIDIOC_G_FMT:\n");
nWidthFinal = fmt.fmt.pix.width;
nHeightFinal = fmt.fmt.pix.height;
printf("set_data_format:finally negotiated width:%d height:%d\n",
nWidthFinal, nHeightFinal);
/* checking what is finally negotiated */
min = fmt.fmt.pix.width * 2;
if (fmt.fmt.pix.bytesperline < min) {
printf
("set_data_format:driver reports bytes_per_line:%d(bug)\n",
fmt.fmt.pix.bytesperline);
/*correct it */
fmt.fmt.pix.bytesperline = min;
} else {
printf
("set_data_format:driver reports bytes_per_line:%d\n",
fmt.fmt.pix.bytesperline);
}
min = fmt.fmt.pix.bytesperline * fmt.fmt.pix.height;
if (fmt.fmt.pix.sizeimage < min) {
printf("set_data_format:driver reports size:%d(bug)\n",
fmt.fmt.pix.sizeimage);
/*correct it */
fmt.fmt.pix.sizeimage = min;
} else {
printf("set_data_format:driver reports size:%d\n",
fmt.fmt.pix.sizeimage);
}
printf("set_data_format:Finally negotiated width:%d height:%d\n",
nWidthFinal, nHeightFinal);
#endif
return 0;
}
/******************************************************************************/
static int init_capture_buffers(void)
{
struct v4l2_requestbuffers req;
int nIndex = 0;
CLEAR(req);
req.count = MIN_BUFFERS;
req.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
req.memory = V4L2_MEMORY_MMAP;
if (-1 == ioctl(fdCapture, VIDIOC_REQBUFS, &req)) {
printf("init_capture_buffers:ioctl:VIDIOC_REQBUFS\n");
return -1;
}
if (req.count < MIN_BUFFERS) {
printf("init_capture_buffers only:"
"%d buffers avilable, can't proceed\n", req.count);
return -1;
}
nBuffers = req.count;
printf("device buffers:%d\n", req.count);
buffers = (struct buffer *)calloc(req.count, sizeof(struct buffer));
if (!buffers) {
printf("init_capture_buffers:calloc:\n");
return -1;
}
for (nIndex = 0; nIndex < req.count; ++nIndex) {
struct v4l2_buffer buf;
CLEAR(buf);
buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
buf.memory = V4L2_MEMORY_MMAP;
buf.index = nIndex;
if (-1 == ioctl(fdCapture, VIDIOC_QUERYBUF, &buf)) {
printf("init_capture_buffers:VIDIOC_QUERYBUF:\n\n");
return -1;
}
buffers[nIndex].length = buf.length;
buffers[nIndex].start =
mmap(NULL, buf.length, PROT_READ | PROT_WRITE,
MAP_SHARED, fdCapture, buf.m.offset);
printf("buffer:%d phy:%x mmap:%p length:%d\n", buf.index,
buf.m.offset, buffers[nIndex].start, buf.length);
if (MAP_FAILED == buffers[nIndex].start) {
printf("init_capture_buffers:mmap:\n");
return -1;
}
}
return 0;
}
/******************************************************************************/
static int start_streaming(void)
{
int i = 0;
enum v4l2_buf_type type;
for (i = 0; i < nBuffers; i++) {
struct v4l2_buffer buf;
CLEAR(buf);
buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
buf.memory = V4L2_MEMORY_MMAP;
buf.index = i;
printf("Queing buffer:%d\n", i);
if (-1 == ioctl(fdCapture, VIDIOC_QBUF, &buf))
printf("start_streaming:ioctl:VIDIOC_QBUF:\n");
}
/* all done , get set go */
printf("VIDIOC_STREAMON\n");
type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
if (-1 == ioctl(fdCapture, VIDIOC_STREAMON, &type))
printf("start_streaming:ioctl:VIDIOC_STREAMON:\n");
return 0;
}
/******************************************************************************/
static int display_bitmap_osd0(void)
{
static unsigned int nDisplayIdx = 1;
static unsigned int nWorkingIndex = 0;
int y;
char *dst;
char *src;
int fd;
//leon test
return 0;
dst = osd0_display[nWorkingIndex];
if (dst == NULL)
return -1;
fd = fd_osd0;
if (rgb565_enable == 1) { /* RGB565 */
src = (char *)rgb16;
for (y = 0; y < test_data.osd0_height; y++) {
memcpy(dst, src, (test_data.osd0_width * 2));
dst += osd0_fixInfo.line_length;
src += (704 * 2);
}
} else if (rgb565_enable == 2) { /* 8 bit bitmap */
src = (char *)test_8;
for (y = 0; y < test_data.osd0_height; y++) {
memcpy(dst, src, (test_data.osd0_width));
dst += osd0_fixInfo.line_length;
src += (704);
}
} else /* 1/2/4 bit bitmap and attribute */
memset(dst, test_data.osd0_coloridx, osd0_size);
nWorkingIndex = (nWorkingIndex + 1) % OSD_NUM_BUFS;
nDisplayIdx = (nDisplayIdx + 1) % OSD_NUM_BUFS;
if ((flip_bitmap_buffers(fd, nDisplayIdx)) < 0)
return -1;
return 0;
}
/******************************************************************************/
static int display_bitmap_osd1()
{
static unsigned int nDisplayIdx = 1;
static unsigned int nWorkingIndex = 0;
int y;
char *dst;
char *src;
int fd;
dst = osd1_display[nWorkingIndex];
if (dst == NULL)
return -1;
fd = fd_osd1;
if (rgb565_enable_osd1 == 1) { /* RGB565 */
src = (char *)rgb16;
for (y = 0; y < test_data.osd1_height; y++) {
memcpy(dst, src, (test_data.osd1_width * 2));
dst += osd1_fixInfo.line_length;
src += (704 * 2);
}
} else if (rgb565_enable_osd1 == 2) { /* 8 bit bitmap */
src = (char *)test_8;
for (y = 0; y < test_data.osd1_height; y++) {
memcpy(dst, src, (test_data.osd1_width));
dst += osd1_fixInfo.line_length;
src += (704);
}
} else /* 1/2/4 bit bitmap and attribute */
memset(dst, test_data.osd1_coloridx, osd1_size);
nWorkingIndex = (nWorkingIndex + 1) % OSD_NUM_BUFS;
nDisplayIdx = (nDisplayIdx + 1) % OSD_NUM_BUFS;
if ((flip_bitmap_buffers(fd, nDisplayIdx)) < 0)
return -1;
return 0;
}
/******************************************************************************/
static int display_frame(char id, void *ptr_buffer)
{
static unsigned int nDisplayIdx = 0;
static unsigned int nWorkingIndex = 1;
int y;
int yres;
char *dst;
char *src;
int fd;
unsigned int line_length;
if (id == VID0) {
yres = test_data.vid0_height;
dst = vid0_display[nWorkingIndex];
if (dst == NULL)
return -1;
fd = fd_vid0;
line_length = vid0_fixInfo.line_length;
}
if (id == VID1) {
yres = test_data.vid1_height;
dst = vid1_display[nWorkingIndex];
if (dst == NULL)
return -1;
fd = fd_vid1;
line_length = vid1_fixInfo.line_length;
}
src = ptr_buffer;
for (y = 0; y < yres; y++) {
memcpy(dst, src, (720 * 2));
dst += line_length;
src += (720 * 2);
}
nWorkingIndex = (nWorkingIndex + 1) % VIDEO_NUM_BUFS;
nDisplayIdx = (nDisplayIdx + 1) % VIDEO_NUM_BUFS;
if ((flip_video_buffers(fd, nDisplayIdx)) < 0)
return -1;
return 0;
}
/******************************************************************************/
static int flip_bitmap_buffers(int fd, int buf_index)
{
struct fb_var_screeninfo var_info;
if (ioctl(fd, FBIOGET_VSCREENINFO, &var_info) < -1) {
printf("flip_bitmap_buffers:FBIOGET_VSCREENINFO\n\n");
return -1;
}
var_info.yoffset = var_info.yres * buf_index;
/* Swap the working buffer for the displayed buffer */
if (ioctl(fd, FBIOPAN_DISPLAY, &var_info) < -1) {
printf("flip_bitmap_buffers:FBIOPAN_DISPLAY\n\n");
return -1;
}
return 0;
}
/******************************************************************************/
static int flip_video_buffers(int fd, int buf_index)
{
int dummy;
struct fb_var_screeninfo var_info;
if (ioctl(fd, FBIOGET_VSCREENINFO, &var_info) < -1) {
printf("flip_video_buffers:FBIOGET_VSCREENINFO\n\n");
return -1;
}
var_info.yoffset = var_info.yres * buf_index;
/* Swap the working buffer for the displayed buffer */
if (ioctl(fd, FBIOPAN_DISPLAY, &var_info) < -1) {
printf("flip_video_buffers:FBIOPAN_DISPLAY\n");
printf("\n");
return -1;
}
return 0;
}
/******************************************************************************/
static int mmap_vid1(void)
{
int i;
vid1_size = vid1_fixInfo.line_length * vid1_varInfo.yres;
/* Map the video0 buffers to user space */
vid1_display[0] = (char *)mmap(NULL, vid1_size * VIDEO_NUM_BUFS,
PROT_READ | PROT_WRITE, MAP_SHARED,
fd_vid1, 0);
if (vid1_display[0] == MAP_FAILED) {
printf("\nFailed mmap on %s", FBVID1_DEVICE);
return FAILURE;
}
for (i = 0; i < VIDEO_NUM_BUFS - 1; i++) {
vid1_display[i + 1] = vid1_display[i] + vid1_size;
printf("Display buffer %d mapped to address %#lx\n", i + 1,
(unsigned long)vid1_display[i + 1]);
}
return SUCCESS;
}
/******************************************************************************/
static int mmap_osd0(void)
{
int i;
osd0_size = osd0_fixInfo.line_length * osd0_varInfo.yres;
/* Map the osd0 buffers to user space */
osd0_display[0] = (char *)mmap(NULL, osd0_size * OSD_NUM_BUFS,
PROT_READ | PROT_WRITE, MAP_SHARED,
fd_osd0, 0);
if (osd0_display[0] == MAP_FAILED) {
printf("\nFailed mmap on %s", OSD0_DEVICE);
return FAILURE;
}
for (i = 0; i < OSD_NUM_BUFS - 1; i++) {
osd0_display[i + 1] = osd0_display[i] + osd0_size;
printf("Display buffer %d mapped to address %#lx\n", i + 1,
(unsigned long)osd0_display[i + 1]);
}
return SUCCESS;
}
/******************************************************************************/
static int unmap_and_disable(char id)
{
switch (id) {
case VID0:
if (munmap(vid0_display[0], vid0_size * VIDEO_NUM_BUFS) == -1) {
printf("\nFailed munmap on %s", FBVID1_DEVICE);
return FAILURE;
}
break;
case VID1:
if (munmap(vid1_display[0], vid1_size * VIDEO_NUM_BUFS) == -1) {
printf("\nFailed munmap on %s", FBVID1_DEVICE);
return FAILURE;
}
break;
case OSD0:
if (munmap(osd0_display[0], osd0_size * OSD_NUM_BUFS) == -1) {
printf("\nFailed munmap on %s", OSD0_DEVICE);
return FAILURE;
}
break;
case OSD1:
if (munmap(osd1_display[0], osd1_size * OSD_NUM_BUFS) == -1) {
printf("\nFailed munmap on %s", OSD1_DEVICE);
return FAILURE;
}
break;
default:
break;
}
return SUCCESS;
}
/******************************************************************************/
static int init_osd0_device(int fd_osd0, struct fb_var_screeninfo *var_info)
{
//vpbe_window_position_t pos;
if (ioctl(fd_osd0, FBIOGET_FSCREENINFO, &osd0_fixInfo) < 0) {
printf("\nFailed FBIOGET_FSCREENINFO osd0");
return FAILURE;
}
/* Get Existing var_screeninfo for osd0 window */
if (ioctl(fd_osd0, FBIOGET_VSCREENINFO, var_info) < 0) {
printf("\nFailed FBIOGET_VSCREENINFO");
return FAILURE;
}
prev_osd0_var = *var_info;
/* Modify the resolution and bpp as required */
var_info->xres = test_data.osd0_width;
var_info->yres = test_data.osd0_height;
var_info->bits_per_pixel = test_data.osd0_bpp;
var_info->vmode = test_data.osd0_vmode;
/* Change the virtual Y-resolution for buffer flipping (2 buffers) */
var_info->yres_virtual = var_info->yres * OSD_NUM_BUFS;
/* Set osd0 window format */
if (ioctl(fd_osd0, FBIOPUT_VSCREENINFO, var_info) < 0) {
printf("\nFailed FBIOPUT_VSCREENINFO");
return FAILURE;
}
/* Set window position */
if (ioctl(fd_osd0, FBIO_SETPOSX, test_data.osd0_xpos) < 0) {
printf("\nFailed FBIO_SETPOSX");
return FAILURE;
}
if (ioctl(fd_osd0, FBIO_SETPOSY, test_data.osd0_ypos) < 0) {
printf("\nFailed FBIO_SETPOSX");
return FAILURE;
}
/* Enable the window */
if (ioctl(fd_osd0, FBIOBLANK, 0)) {
printf("Error enabling OSD0\n");
return FAILURE;
}
return SUCCESS;
}
/******************************************************************************/
static int init_vid1_device(int fd, struct fb_var_screeninfo *var_info)
{
if (ioctl(fd, FBIOGET_FSCREENINFO, &vid1_fixInfo) < 0) {
printf("\nFailed FBIOGET_FSCREENINFO vid1");
return FAILURE;
}
/* Get Existing var_screeninfo for vid1 window */
if (ioctl(fd, FBIOGET_VSCREENINFO, var_info) < 0) {
printf("\nFailed FBIOGET_VSCREENINFO");
return FAILURE;
}
prev_vid1_var = *var_info;
/* Modify the resolution and bpp as required */
var_info->xres = test_data.vid1_width;
var_info->yres = test_data.vid1_height;
var_info->vmode = test_data.vid1_vmode;
var_info->bits_per_pixel = test_data.vid1_bpp;
/* Change the virtual Y-resolution for buffer flipping (3 buffers) */
var_info->yres_virtual = var_info->yres * VIDEO_NUM_BUFS;
/* Set vid1 window format */
if (ioctl(fd, FBIOPUT_VSCREENINFO, var_info) < 0) {
printf("\nFailed FBIOPUT_VSCREENINFO");
return FAILURE;
}
/* Set window position */
if (ioctl(fd_vid1, FBIO_SETPOSX, test_data.vid1_xpos) < 0) {
printf("\nFailed FBIO_SETPOS");
return FAILURE;
}
if (ioctl(fd_vid1, FBIO_SETPOSY, test_data.vid1_xpos) < 0) {
printf("\nFailed FBIO_SETPOS");
return FAILURE;
}
/* Enable the window */
if (ioctl(fd_vid1, FBIOBLANK, 0)) {
printf("Error enabling VID1\n");
return FAILURE;
}
return SUCCESS;
}
/******************************************************************************
* Example to show vid1 in YUV format, OSD0 in RGB565 format and
* OSD1 is attribute format.
******************************************************************************/
static int vpbe_UE_1(void)
{
rgb565_enable = 1;
rgb565_enable_osd1 = 0;
v4l2_std_id cur_std;
int ret = 0;
/* Setup Capture */
if (initialize_capture(&cur_std) < 0) {
printf("Failed to intialize capture\n");
return ret;
}
DBGENTER;
#if 0
if (cur_std & V4L2_STD_NTSC) {
test_data.vid1_width = WIDTH_NTSC;
test_data.vid1_height = HEIGHT_NTSC;
} else {
test_data.vid1_width = WIDTH_PAL;
test_data.vid1_height = HEIGHT_PAL;
}
#endif
test_data.vid1_width = WIDTH_VGA;
test_data.vid1_height = HEIGHT_VGA;
test_data.vid1_bpp = 16;
test_data.vid1_vmode = FB_VMODE_INTERLACED;
test_data.vid1_xpos = 0;
test_data.vid1_ypos = 0;
test_data.vid1_hzoom = 0;
test_data.vid1_vzoom = 0;
test_data.osd0_width = 150;
test_data.osd0_height = 150;
test_data.osd0_bpp = 16;
test_data.osd0_hzoom = 0;
test_data.osd0_vzoom = 0;
test_data.osd0_xpos = 10;
test_data.osd0_ypos = 10;
#if 0
if (cur_std & V4L2_STD_NTSC)
change_sysfs_attrib(ATTRIB_MODE, DISPLAY_MODE_NTSC);
else
change_sysfs_attrib(ATTRIB_MODE, DISPLAY_MODE_PAL);
#endif
if (display_out) {
if ((init_vid1_device(fd_vid1, &vid1_varInfo)) < 0) {
printf("\nFailed to init vid1 window ");
return FAILURE;
}
if ((init_osd0_device(fd_osd0, &osd0_varInfo)) < 0) {
printf("\nFailed to init osd0 window ");
return FAILURE;
}
if (mmap_vid1() == FAILURE)
return FAILURE;
if (mmap_osd0() == FAILURE)
return FAILURE;
}
printf("Starting loop..........\n");
start_loop();
/* unmap video buffers */
if (display_out) {
if (unmap_and_disable(VID1) < 0)
return FAILURE;
if (unmap_and_disable(OSD0) < 0)
return FAILURE;
}
DBGEXIT;
return SUCCESS;
}
/******************************************************************************/
static void close_all_windows(void)
{
if (fd_vid0)
close(fd_vid0);
if (fd_vid1)
close(fd_vid1);
if (fd_osd0)
close(fd_osd0);
if (fd_osd1)
close(fd_osd1);
}
/******************************************************************************/
static int open_all_windows(void)
{
if ((fd_vid0 = open(FBVID0_DEVICE, O_RDWR)) < 0)
goto open_all_exit;
if ((fd_vid1 = open(FBVID1_DEVICE, O_RDWR)) < 0)
goto open_all_exit;
if ((fd_osd0 = open(OSD0_DEVICE, O_RDWR)) < 0)
goto open_all_exit;
if ((fd_osd1 = open(OSD1_DEVICE, O_RDWR)) < 0)
goto open_all_exit;
return SUCCESS;
open_all_exit:
close_all_windows();
return FAILURE;
}
/*******************************************************************************
* Function will use the SysFS interface to change the output and mode
*/
static int change_sysfs_attrib(char *attribute, char *value)
{
int sysfd = -1;
char init_val[32];
char attrib_tag[128];
bzero(init_val, sizeof(init_val));
strcpy(attrib_tag, "/sys/class/davinci_display/ch0/");
strcat(attrib_tag, attribute);
sysfd = open(attrib_tag, O_RDWR);
if (!sysfd) {
printf("Error: cannot open %d\n", sysfd);
return FAILURE;
}
printf("%s was opened successfully\n", attrib_tag);
read(sysfd, init_val, 32);
lseek(sysfd, 0, SEEK_SET);
printf("Current %s value is %s\n", attribute, init_val);
write(sysfd, value, 1 + strlen(value));
lseek(sysfd, 0, SEEK_SET);
memset(init_val, '\0', 32);
read(sysfd, init_val, 32);
lseek(sysfd, 0, SEEK_SET);
printf("Changed %s to %s\n", attribute, init_val);
close(sysfd);
return SUCCESS;
}
/******************************************************************************
* Function disables all the four windows to ensure no
* window inter-dependency
*/
static int disable_all_windows(void)
{
int fd;
// Disbale OSD0
fd = open(OSD0_DEVICE, O_RDWR);
if (!fd) {
printf("Error: cannot open OSD0\n");
return -1;
}
if (ioctl(fd, FBIOBLANK, 1)) {
printf("Error disabling the window OSD0\n");
return -2;
}
close(fd);
// Disbale OSD1
fd = open(OSD1_DEVICE, O_RDWR);
if (!fd) {
printf("Error: cannot open OSD1\n");
return -1;
}
if (ioctl(fd, FBIOBLANK, 1)) {
printf("Error disabling the window OSD0\n");
return -2;
}
close(fd);
// Disbale VID0
fd = open(FBVID0_DEVICE, O_RDWR);
if (!fd) {
printf("Error: cannot open VID0\n");
return -1;
}
if (ioctl(fd, FBIOBLANK, 1)) {
printf("Error disabling the window VID0\n");
return -2;
}
close(fd);
// Disbale VID1
fd = open(FBVID1_DEVICE, O_RDWR);
if (!fd) {
printf("Error: cannot open VID1\n");
return -1;
}
if (ioctl(fd, FBIOBLANK, 1)) {
printf("Error disabling the window VID1\n");
return -2;
}
close(fd);
return SUCCESS;
}
/*******************************************************************************
* menu function
*******************************************************************************/
void menu(void)
{
printf("Usage: fbdev_loopback -s <flag>\n");
printf("flag = 0 for infinite loop, 1 - for 500 frames\n");
}
/******************************************************************************/
/* main function */
int main(int argc, char *argv[])
{
int ret = 0, d, index;
char shortoptions[] = "s:d:w:p:";
DBGENTER;
for (;;) {
d = getopt_long(argc, argv, shortoptions, (void *)NULL, &index);
if (-1 == d)
break;
switch (d) {
case 's':
case 'S':
stress_test = atoi(optarg);
break;
case 'd':
case 'D':
display_out = atoi(optarg);
break;
case 'w':
case 'W':
save_frame = atoi(optarg);
break;
case 'p':
case 'P':
print_fn = atoi(optarg);
break;
default:
menu();
exit(1);
}
}
if (display_out) {
if (open_all_windows() != 0) {
printf("Test fail\n");
return 0;
}
}
ret = vpbe_UE_1();
if (display_out) {
restore_config();
close_all_windows();
}
close(fdCapture);
DBGEXIT;
return ret;
}
Dear sir,
I tried to run one application ipipe application it is running correctly and i get the exe if i tried to run the code in the board it is showing the below error.
./ipipe: error while loading shared libraries: libposixtime.so.1: cannot open shared object file: No such file or directory
Dear sir,
In dm355 what is the maximum pixel rate of picture.720p is possible. It is possible to take 1080p?.I am using 5mp camera.