Other Parts Discussed in Thread: OMAP-L138
Hi,
I am using omap-l138. To load the images in nand flash I am using lauterbach LA-7708. It is loading the images in nand but when I start the board I am getting this error:
Booting with TI UBL
Device OPP (300MHz, 1.2V)
U-Boot 2012.04.01-svn30 (Jun 27 2012 - 10:05:06)
I2C: ready
DRAM: 128 MiB
WARNING: Caches not enabled
NAND: 512 MiB
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
In: serial
Out: serial
Err: serial
SF: Detected M25P64 with page size 64 KiB, total 8 MiB
Default using MAC address from environment
Default using MAC address from environment
Net: DaVinci-EMAC
Hit any key to stop autoboot: 0
Loading from nand0, offset 0x500000
NAND read from offset 500000 failed -74
** Read error
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.37+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2314908 Bytes = 2.2 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
U-Boot >
Here I am trying to load kernal image in omap-l138 evm.
Env. variables given as :
bootargs=root=/dev/ram0 rw initrd=0xc2000000,32M console=ttyS2,115200b8 ramdisk_size=32768K
bootcmd=nand read 0xc2000000 0xA00000 0xC65D40; nboot 0xc0700000 0 0x100000; bootm 0xc0700000
The same images are booting up the board using tftpboot, ramboot and even when I am loading the images through tftp and booting using nand boot.
But my requirement is to load the images in nand flash using Lauterbach.
Please help. Thanks in advance...