I'm using the second i2c channel to connect to HDMI transmitter sii9022a. In order to get EDID information from the attached monitor the sii9022a chip passes i2c request direct to the monitors i2c bus. To return to sii9022a mode one has to write data to HDMI transmitter, but this data won't be acknowledged. Because of this i2c produces timeout permanently (omap_i2c omap_i2c.2: controller timed out), so no communication is possible.
the HDMI chip has i2c address 0x72 (8-bit notation) and EDID channel 0xa0 (8-bit notation). AFAIK there is only one device at a time on the bus, i.e. as soon as I switch sii9022a to access monitor only 0xa0 responds to the queries. And I need to send a message to 0x72 ignoring normal i2c conditions in order to turn it back in normal mode.
The driver for this HDMI transmitter can be found here: http://gitorious.org/efikamx/linux-kernel.git (drivers/video/mxc/siihdmi.c)
How can I send this write request without awaiting for ACK?
Yegor