If the following interfaces (SRIO, PCIE, GbE, Hyperlink, TSIP, EMIF16, SPI, Timer0, 1, UART CTS and RTS) are not used in the hardware design, how should they be terminated? Not connected or terminated to ground or other voltages
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the following interfaces (SRIO, PCIE, GbE, Hyperlink, TSIP, EMIF16, SPI, Timer0, 1, UART CTS and RTS) are not used in the hardware design, how should they be terminated? Not connected or terminated to ground or other voltages
Hi Wenjun,
you'll find the answers in the HW Design Guidelines:
http://www.ti.com/lit/an/sprabi2b/sprabi2b.pdf
Kind regards,
one and zero
Thanks for directing. The answer is mainly left floating, or pulled low or high to reduce leakage current for some of the interfaces.