This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change IP address in NFS

Guru 20755 points
Hello, Is it legal to change ip address & mac address when working with NFS, after linux finished startup ? It seems that in such case, NFS can get stuck, right? Thank you, Ran
  • My guess is that changing the address would cause a momentary interruption in networking, which might upset the NFS mount and possibly hang the system. It seems like a reasonably simple thing to try out, though. You could set up a large filecopy that runs while you do it, which would be a bit of a stress test.