Other Parts Discussed in Thread: MATHLIB
hello,everybody.
I use C67xmathlib_2_01_00_00_Windows_Setup.exe in order to speed up the computation.
my Build Properties as follows:
ccs4.1.2.00027
CGT:6.1.12
Propertiers->C6000 Linker->File Search Path->(--library)->Add->C:\c67xmathlib_2_01_00_00\lib\c674xfastMath.lib->Move Up。
Propertiers->C6000 Linker->File Search Path->(--search_path)->Add->C:\c67xmathlib_2_01_00_00\lib->Move Up。
Propertiers->C6000 Compiler->Include Options->(--include)->Add->C:\c67xmathlib_2_01_00_00\inc.
Test program:
#include <c67fastmath.h>
void main()
{
double a = 232.2312;
double b = rsqrtdp(a);
double c = sqrt(a);
}
Result:
a = 232.2312;
b = 0.065620527447;
c = -1074409180.0;
I don't why the error analysis.
Is not configured properly or version does not correspond to??
Who can guide me.Thanks.
Who can provide a can I use to mathlib base on CCS4.1.2.