This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148's C674x internal memory performance issue

Hi,
I am moving my code from C64x+ (on DM6437) to C674x (on DM8148 and J5). But the performance numbers were actually coming worse.
So I tried to check the L1D, L2 and DDR access times. I have written a sample code to count the DSP cycles taken in doing a memory transfer between these memories. (I have attached the source file and the RTSC configurations I am using.)
I am getting the following cycle counts on the different platforms:

From -> To    | DM6437 | DM8148 | J5 EVM | % increase on DM8148 | % increase on J5 EVM
---------------------------------------------------------------------------------------------------------------------------

L1D -> L1D    | 4477        | 4561       | 6488      | 1.88%                               | 44.92%
L2 -> L2          | 8030        | 10680    | 36967    | 33.00%                             | 360.36%
DDR -> DDR  | 310139   | 525073  | 641351  | 69.30%                             | 106.79%
===========================================================================
I am not understanding why the numbers have increased on DM8148 and J5.
Also, the DDR performance is coming out to be worse
inpite of improved DDR type(DDR3) and DDR clock frequency ?

Please help.

- Abhishek Gupta

About the test code:
- I am doing a memcpy() of 16kB of data from L1D to L1D, L2 to L2 and DDR to DDR.
- This was run on 3 different platforms: DM6437, DM8148 Centaurus and J5 EVM.
- The project is built in CCS5.1 (CGTools version: 7.3.1).
- The base addresses of L1D, L2 mentioned are for DM8148/J5. They were changed appropriately for DM6437.
- Cache is disabled on all platforms. I have attached snapshots of the RTSC platform file creation wizard in CCS5.1.
- DDR frequency on DM6437= 162MHz, and on DM8148/J5 = 333MHz
- DSP Clock Frequency on DM6437= 594MHz, and on = 500MHz

L2_access_test.zip