This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in Building filesystem

Hello TI,

                        I am using  TI_Android_ICS_4Sources android stack  in AM37x , i done all the boot images but i cant build the Filesystem  its showing following error, 

 Could you please solve this issue..

root:~/Desktop/ICS/TI-Android-ICS-4.0.3_AM37x_3.0.0# make TARGET_PRODUCT=omap3evm OMAPES=5.x -j4
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.0.3
TARGET_PRODUCT=omap3evm
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=IML74K
============================================
Checking build tools versions...
************************************************************
You are attempting to build with the incorrect version
of java.

Your version is: java version "1.6.0_23".
The correct version is: Java SE 1.6.

Please follow the machine setup instructions at
http://source.android.com/source/download.html
************************************************************
build/core/main.mk:131: *** stop. Stop.



Thanks in advance

Bhagavath ram